Skip to main content
Visitor II
February 3, 2016
Question

STM32F4 disco + MEMS microphone array

  • February 3, 2016
  • 0 replies
  • 601 views
Posted on February 03, 2016 at 10:44

Hello, my project involves capturing the data from a MEMS microphone array. I found one article which describes, that it is possible to achieve this with a STM32F4 processors, so I would use STM32F407 discovery board. I added the diagram in the attachment. It shows, that the input clock (12.288MHz) is divided and outputed to the MEMS microphone array and also to trigger the DMA. As I understand, the clock passed to the array should be N times smaller than the one passed to DMA, where N is the microphone count. But is it possible to output two different clock from one timer. And if not would it work if I used to timers which were clocked from the same source (for example APB2) and outputed the to MEMS array and DMA respectively? Would the DMA work in sync with the array?

#mems-microphone-array #stm32f4
    This topic has been closed for replies.