STTS22H - I2C Address Setting
Hello,
In the data sheet of the sensor (https://www.st.com/resource/en/datasheet/stts22h.pdf), it's mentioned that to set the Address we need to connect the ADDR pin whether to VDD (to have the address 0111000) or to GND (to have the address 0111111), these only two address are mentioned as the only possibilities
But in the Evaluation Board documentation (https://www.st.com/resource/en/data_brief/steval-mki200v1k.pdf), the ADDR pin is pulled up to VDD by a resistor, and four values of the resistor are mentioned to select one of four different addresses .
can you please clarify which is the right way to set the I2C address?
thanks in advance