STTS22H I2C addressing
Hello,
I have started working on the STTS22H and noticed that, at least for my part, the datasheet I2C addressing directive seems to be inverted. Aside from the fact that the datasheet and the evaluation kit have different addressing directives, the evaluation kit seems to have the ADDR pin connected to VDD which would mean the 7-bit address is 0111 000. However, when testing out the sensor it would only respond when using the 7-bit address 0111 111, which is the configuration for when the ADDR pin is connected to ground as pointed out in the snapshot from the datasheet below.
Could that mean that there is an issue with the datasheet or could that be an issue with the kit I have got?
On another unrelated topic, what is the default value of if_add_inc in the CTRL register on boot?
Thanks.