Suggest me an accelerometer sensor for speed calculation of moving vehicle.Dynamic values of an accelerometer.
I want to use an accelerometer to calculate the speed of a moving vehicle. For this i need a accelerometer which should give _ve values(2's complement) in Deceleration and +ve values in (2's complement) in acceleration. It should have 2g range with 12bit(or more) resolution. with less noise affected. It should have less Zero offset error.
If there is any sensor Please Suggest me one.
Thank you in Advance.