tap detection doesn't work
Hello,
I am trying to use the LSM to detect taps . I use the default configuration which suggested in the application notes :
1. Write 60h to CTRL1_XL // Turn on the accelerometer
// ODR_XL = 417 Hz, FS_XL = ±2 g
2. Write 0Eh to TAP_CFG0 // Enable tap detection on X, Y, Z-axis
3. Write 0Ch to TAP_CFG1 // Set X-axis threshold and axes priority
4. Write 8Ch to TAP_CFG2 // Set Y-axis threshold and enable interrupt
5. Write 0Ch to TAP_THS_6D // Set Z-axis threshold
6. Write 7Fh to INT_DUR2 // Set Duration, Quiet and Shock time windows
7. Write 80h to WAKE_UP_THS // Single-tap and double-tap enabled (SINGLE_DOUBLE_TAP = 1)
8. Write 08h to MD1_CFG // Double-tap interrupt driven to INT1 pin With this configuration i am able to get interrupts. My problem starts when i try to check the cause of the interrupt by reading TAP_SRC or ALL_INT_SRC.
When i read ALL_INT_SRC register i see that the cause of the interrupt was Wake-up event(WU_IA) which should be disabled as far as i understand from the configuration above( WAKE_UP_THS = 0x80).
When i read TAP_SRC register i see that there was TAP event detection on one of the axis, but the bit's for SINGLE_TAP / DOUBLE_TAP / TAP_IA are all zero's. I would expect to get the SINGLE_TAP / DOUBLE_TAP bit's set.
Any suggestion on what may cause this not to work as expected ?
Thanks,
David.