Temperature characteristics of IIS2DLPC
I am making a simple inclinometer using IIS2DLPC. The 'Zero-g offset change vs. temperature' of IIS2DLPC is specified as a maximum of ±1mg/℃, but some of the boards I made have reached 2.93mg/℃.
Some have relatively good values of 0.3-0.4mg/℃, while others have values of 0.8-1.6mg/℃, so the characteristics vary.
2.93mg/℃ is the worst value evaluated.
Since most of the units can be measured cleanly, I think that it is not a problem with the circuit board, but some external factor is at work. Please let me know if there are any possible factors.
Note that the measurements are taken only on the printed circuit board, without being assembled into a case.