Skip to main content
Visitor II
May 14, 2018
Question

Temperature sensor on ISM330DLC

  • May 14, 2018
  • 2 replies
  • 1094 views

Posted on May 14, 2018 at 16:11

Hello, can you please tell if the temperature sensor on ISM330DLC returns absolute temperature values or the difference values with respect to a reference? Just read a thread (

https://community.st.com/0D50X00009XkXfjSAF

) that mentions 'difference with respect to a reference' so wanted to confirm if the same is happening for ISM330DLC as well.

Best regards,

Ankur

    This topic has been closed for replies.

    2 replies

    ST Employee
    May 14, 2018
    Posted on May 14, 2018 at 16:53

    Here are the temperature sensor characteristics from the device datasheet.

    As you can see the sensors measure difference values with respect to reference 25°C. The offset can be up to +/- 15°C.

    0690X0000060KkGQAU.png
    Visitor II
    May 15, 2018
    Posted on May 15, 2018 at 07:41

    Thanks Miroslav. So if we have multiple devices with this sensor, every device can have a different temperature offset, correct?

    ST Employee
    May 15, 2018
    Posted on May 15, 2018 at 22:08

    Yes, it is correct.

    Visitor II
    May 16, 2018
    Posted on May 16, 2018 at 13:58

    Thanks Miroslav!