Teseo GNSS module - no fix
Hi,
I have own design with Teseo GNSS LV3R module. It is connected to STM32L071. After power up I just set Reset pin to low for 10 ms and then I keep it in high level. Unfortunatelly even after 3 hours under open air ( without clouds and nearby buildings) I still can no read any gps position. The NMEA messages goes but they are almost empty...
My design is inclosed. Did I missed anything? What could I make wrong?
I tried it with and without the LNA - the result was same.
Thank you very much for advices.
Jan.