Skip to main content
Visitor II
July 10, 2019
Question

The interface firmware FAILED to reset/halt the target MCU FAIL.TXT message on my STEVAL-IDP005V1. How do I fix this?

  • July 10, 2019
  • 1 reply
  • 883 views

I have connected STEVAL-IDP005V1 sensor board (it has an STM32F469AI ARM® Cortex®-M4 32-bit MCU on it) to the ST-LINK/V2-1 programmer/debugger on stm32 NUCLEO-F401RE board via an adapter board STEVAL-UKI001V1. When I connect the USB cable to the PC and st-link/v2-1, I see the file 'FAIL.txt' saying 'The interface firmware FAILED to reset/halt the target MCU'.

Can someone help me in fixing this? Thanks in advance

-Chandrasekhar DVS

    This topic has been closed for replies.

    1 reply

    ST Employee
    July 31, 2019

    ​Hi, are you using the STM32 ST-LINK Utility for the debug? If so, you can do a chip erase and re-connect to the target. regards

    ChanduAuthor
    Visitor II
    August 2, 2019

    Hi @Eleon BORLINI​ ,

    The thing is, the USB drive which is supposed to show me available space of 2MB(as claimed by STEVAL-IDP005V1 sensor board) when I connect it to PC is not showing. I think this is to be fixed first. I tried checking the power management system to see if the power supply is right. Any other Ideas you can give me to first see a 2MB space available to dump the .bin file?

    Thanks in advance,

    -Chandrasekhar DVS