The interrupt on LIS2MDL doesn't trigger.
I would like to have an interrupt thank to a threshold. So I have used CFG_REG_C (0x62) to enable interrupt on pin and INT_CTRL_REG to configure it (see screenshot). However, the interrupt is never trigger, so I have readen INT_SOURCE_REG each 500 ms, and we can see that there is interrupt (last bit) and the threshold is exceeded on differents axes, but I have never had interrupt on pin.