The LIS3DH crash test reads an abnormal acceleration value
When I was doing impact testing, using the 16g range, with my device gently knock on the desktop, the acceleration values read have acceleration values of more than 10g, a bit unbelievable, acceleration reading and conversion are in accordance with In the manual, there should be no problem. When the plane is laid flat, the X and Y axes tend to be 0, and the z axis is about 1G. What causes this?