The magnetic sensor of STEVAL-MKI173V does not enter the data ready state by I2C communication.
Wrote 0x40 to the CTRL1_A register, wrote 0x8C to the CFG_REG_A_M register.
I was able to read the data on the accelerometer via I2C communication, but the magnetic sensor cannot read it.
How do I change the "Zyxda" bit in the magnetic sensor's STATUS_REG_M to 1?
Please tell me.
Upon examination, I found that the "Zyxda" bit of the magnetic sensor's STATUS_REG_M did not become 1.
There was no error in the I2C communication itself.
In addition, I2C communication was performed according to the communication format of LSM303AH.