Skip to main content
Visitor II
January 31, 2022
Solved

The problem of connecting the STEVAL-MKI209V3 with ISM330DHCX to the computer.

  • January 31, 2022
  • 2 replies
  • 958 views

Hello! I need help.

I'm using windows 10. To work, I downloaded the latest version of Unico-GUI.

The following error occurs.

0693W00000JNx49QAD.pngMaybe I need to install drivers for the ISM330DHCX module ?

    This topic has been closed for replies.
    Best answer by AG.8

    Hi @ABeze.1​ , probably you didn't updated the firmware (I see it is V2.18.6, probably the default one). You have to program the board with the .bin file you find in the package folder \FIRMWARE\ProfiMEMSTool board (at lease version V3.2x.xx)

    Here there is a guide on how to do it --> https://community.st.com/s/question/0D53W0000057tYrSAI/using-lsm6dso-on-stevalmki109v3-with-unico-gui-9710

    AG

    2 replies

    AG.8Answer
    Visitor II
    January 31, 2022

    Hi @ABeze.1​ , probably you didn't updated the firmware (I see it is V2.18.6, probably the default one). You have to program the board with the .bin file you find in the package folder \FIRMWARE\ProfiMEMSTool board (at lease version V3.2x.xx)

    Here there is a guide on how to do it --> https://community.st.com/s/question/0D53W0000057tYrSAI/using-lsm6dso-on-stevalmki109v3-with-unico-gui-9710

    AG

    ABeze.1Author
    Visitor II
    February 11, 2022

    Thank you very much for your help!

    I updated the firmware and the module successfully connected.

    Best regards

    Anton