Skip to main content
Visitor II
February 6, 2024
Solved

tolerance of IMU internal clock sampling frequency

  • February 6, 2024
  • 1 reply
  • 983 views

Hi,

I am using IMU sensor LSM6DSO set to 100 Hz sampling rate. I am trying to figure out what is the tolerance of the IMU sampling frequency set by it's internal clock. How confident can I be that when I set it to 100 Hz, it will not fluctuate to higher/lower frequencies?

    This topic has been closed for replies.
    Best answer by Federica Bossi

    Hi @zce ,

    From characterization data, and thus not guaranteed in production, the ODR Error percentage is between +/- 15%.

    1 reply

    Technical Moderator
    February 7, 2024

    Hi @zce ,

    From characterization data, and thus not guaranteed in production, the ODR Error percentage is between +/- 15%.