Trouble getting sensortile working with small cradle
Not sure if I'm in the right place for this question, but I recently started using the sensortile development kit for a class/project. I've done all the tutorials with the sensor mounted to the expansion cable. However, now my project requires the sensor to be mounted to the small battery powered cradle/case.
I purchased an addition sensortile (STEVAL-STLCS02V1 solder only) for this use so that I had the original to still test things with on the expansion board. So I've soldered the new tile to the cradle and it looks like all the connections are solid. However, when I try to see if it works (by building/debugging datalog project from tutorial 1) I get a "Wrong Device Detected" error.
I'm pretty new at this stuff (hence the class), so I'm just trying to figure out where to go from here. How do I know if the sensortile is mounted to the cradle properly? Is this error due to that, or something else?
Any help or advice would be appreciated. Thanks.