Trying to use magnetometer II2SMDC to get angle of rotation of a plan
Hello,
I'm using the mems II2SMDC from where I get X, Y and Z values.
- I set ODR to 100Hz, COMP_TEMP_EN to 1 and MD_CONTINOUS to 1 for CFG_REG_A (note that low power is disable)
- I set DRV_IIS2MDC_LPF to 1 for CFG_REG_B
- I set DRV_IIS2MDC_BDU to 1 for CFG_REG_C
- I also enable offset cancelation (DRV_IIS2MDC_OFF_CANC) in CFG_REG_B because otherwise values are completly random / wrong.
I'm using X and Y to get an angle on the plan (X, Y) using atan2.
(In fact I'm using X and Z because I attached the mems to a door to detect opening, closing but it does not matter)
My algorithm is a lot inspired from this post : https://arduino.stackexchange.com/questions/18625/converting-three-axis-magnetometer-to-degrees)
Here is my function which converts from X, Y and Z raw values to angles in degrees :
static double main_calculate_angle_degree(int16_t x, int16_t y){
double angle;
angle = atan2((double)y, (double)x);
if (angle >= 0) {
angle = angle * (180 / M_PI);
}
else {
angle = (angle + 2 * M_PI) * (180 / M_PI);
}
return angle;
}
Here is my algorithm :
I have an offset which makes x = 0 in default position. This offset is applied to all axes ( I tried without this offset and it makes no difference )
Some observations :
When angle = 0° : X² + Y² = 2² + 35² = 1229 (X is the average of 5 X values and the same for Y) Then I rotate my mems of 90°, the angle displayed by my device is around 70° : X² + Y² = 300² + 103² = 100609. I guess the value should always be the same because I am just rotating the magnetometer.
Moreover the result is wrong because East (0°) is not "aligned" with West (180°) . What I means is that when my algorithm says 180° I have rotate my mems from lots less or lots more. In fact there is not an angle of 90° between any "axes" (N, S, E or W).
My real problem is that my angle is not moving "linearly". For example, in the image below, between North and East, with atan2 I get 270° which is obviously wrong regarding to the direction.
I added the image of what I see.
diagram starts with East : angle = 0°. South is draw when angle = 90°.