Two iss3dwb sensors - can't choose
Hi there fellas, i got me two Steval-Stwincsv1 and i'm now using the HSDataLog. Everything works perfectly when only one of the sensors is plugged on to the Computer. When i plug the second one and start it, one of them start, and ONLY ONE. It seems like that, i cannot choose which one of them am i triggering. My question is: How am I supposed to choose the sensor which i want the data from, because i cannot seem to be able to choose COM port or do something with the .json config files?