UM2116 NOT Updated with MKI239A Info (“number of data bytes coming after *start” and "setdb")
Hi,
I am using MKI109V3 with Unico Lite and MKI239A. Following UM1064, I need to edit the source code to add MKI239 as additional evaluation board for a combo of acclerometer and gyroscope.
The UM1064, user manual of Unico Lite, suggests to find “number of data bytes coming after *start” and "setdb" from UM2116. But the relevant information for MKI239A is not included in UM2116/Table 4 "Returned values for *start command".
May I kindly ask if this information could be provided? Thanks a lot! I am trying to make everything work before Christmas.
P.S. Below are two screenshot from UM1064 (Section 1 and Section 3.1), showing it is supposed to be straightforward to add new evaluation boards, as long as info is provided in UM2116 table 4...