Skip to main content
Visitor II
March 22, 2021
Solved

Unable to initialize MotionGC.

  • March 22, 2021
  • 1 reply
  • 1164 views

Hi,

I am unable to initialize MotionGC library, since the function MotionGC_Initialize(&val) does not stop execution (pretty much like an infinite loop).

Checking on the User Manual (UM2181), it is stated as a note regarding this function that " the CRC module in STM32 microcontroller (in RCC peripheral clock enable register) has to be enabled before using the library".

Is this the root of the problem and if so, which is the RCC peripheral clock enable register?

    This topic has been closed for replies.
    Best answer by Miroslav BATEK

    Yes. it is most probably root cause of your problem.

    If you use STM32 HAL drivers you need to enable CRC peripheral i.e. using HAL_CRC_Init().

    1 reply

    ST Employee
    March 22, 2021

    Yes. it is most probably root cause of your problem.

    If you use STM32 HAL drivers you need to enable CRC peripheral i.e. using HAL_CRC_Init().

    PMach.1Author
    Visitor II
    March 24, 2021

    You're totally right. It did solve the problem.

    Many thanks. Cheers!