Unico GUI Crashes
Hello all. I've tried to run the latest version of Unico GUI (5.0) by downloading it using the 'Get Software' button at the bottom of this webpage -
. I've installed the GUI by running Setup_Unico_5.0.0.0.exe and installed the driver by running VCP_V1.4.0_Setup.exe. Unfortunately, whenever I run Unico to evaluate LIS3DH (STEVAL-MKI105V1) on my 64 bit Windows 7 machine the program crashes on me. Any idea why this might be happening? This occurs right after I do the following:
- Run C:\Program Files (x86)\STMicroelectronics\Unico\bin\unico.exe- Select STEVAL-MKI105V1 (LIS3DH)- Ensure 'Automatic Port Detection [Enabled]' is checked- Click the 'Select Device' buttonWhen I do this I get a generic 'Cross-platform UI for MEMS demo kits has stopped working' Windows dialog.A couple notes:
- After I run VCP_V1.4.0_Setup.exe and plug our STEVAL-MKI105V1 evaluation board into my computer's USB port Windows Device Manager shows the virtual COM port 'STMicroelectronics Virtual COM Port (COM26)'- Unico GUI version 1.0.0.0 works fine on a Windows XP machine we have with this same evaluation board. This XP machine is using the latest version of the driver (Virtual COM port driver v1.4.0)