Unico-GUI doesn't update X-axis for LIS2DUX12 (MKI109V3 + MKI238A)
Unico Version: 9.17.2.10
FW: V3.60.7
HW: MKI109V3 + MKI238A
OS: Win10
Hi,
Can someone explain how the X/Y/Z axis on Unico are related to the OUT_X/Y/Z_H/L register readouts from the LIS2DUX12? On first glance, it looked like X-axis is not getting updated at all (I've tried with two MKI238A units, same results), but after looking closer at the register readout, it seemed like Y = OUT_X, Z = OUT_Y, and I have no idea where X came from or where OUT_Z went.

What I see on the plots - no movement on X-axis, no matter how much I shook it.

Controls are set to "Easy Configuration"

Register settings and readouts.

Comparing OUT_X/Y/Z registers and what Unico displays. X_OUT was 0xFCB0 = -848, which was close to 'Y', and Y_OUT was 0xF190 = -3696, which was close to 'Z'. I couldn't tell where the "X=13" came from, and it never moved.