Unico & Multiple Decision Trees & UCF - process to use externally generated Decision Tree files
Hi,
Using UNICO (v9.10.0.0), the process to generate a UCF file with multiple Decision Trees seems to be:
1. Load all the test data for ALL Decision Trees, labelling each data set as you would for an individual Tree (presumably the labels need to be unique across all trees)
2. Use the MLC Configuration Tool
3. When it gets to the part about multiple decision trees, enter the number required.
4. Select all the Features required across all the Trees
5. For each tree, select the labels entered in step 1 that are to be grouped into that tree
6. At the generate step it will generate a Decision Tree file for each Tree, and then only one UCF file.
Is that correct?
What are the implications/constraints/issues when generating a UCF with multiple Decision Trees if one or all of them are generated external to UNICO, or if a UNICO DTree has been modified (eg a Node value/threshold changed)?
- Do all the Features specified in the Decision Tree files need to be the same and in the same order? (ie listed in the DTree file after "features:")
- Do the Feature instance numbers (ie "x" in Fx_<feature>_<axis>) have to be aligned (eg F7_PeakToPeak_on_ACC_V)
Thanks,
Brendon.
PS Had the multiple Decision Tree process changed from Unico V9.8?