[URGENT] Use of a Quad Differential Tx/Rx for transmitting (SPI) MEMS sensor data over <3m distance to STM32G4
Hello Community!
We are building a Condition monitoring platform, and need to interface a MEMS based Accelerometer with the STM32G4 at a distance of 3M. I would like to know if someone has had first-hand experience using Quad Differential Drivers & Receivers for transmitting the SPI over Differential line & then interfacing the TTL with STM32.
Also feel free to suggest to me any alternative approach for transmitting SPI over a distance of 2-3m. Data rates are low (6KB/s) & one way from the sensor to the MCU. We can invest in good quality cables (Shielded & twisted pairs)
Quad Differential Drivers & Reveicers I am considering are:
Driver: 4/0 AM26LS31
Receiver: 0/4 AM26LS32
Regards