Skip to main content
Visitor II
November 14, 2018
Question

USB Device HS-IN-FS does NOT work

  • November 14, 2018
  • 0 replies
  • 621 views

I am using STM32Cube_FW_F4_V1.21.0.This is very excellent software.UART,SPI,I2S,RTC,,,work fine but HS-IN-FS.

I have checked HS and FS works fine.

My target board is STM32469I-EVAL board and I'm using EWARM compiler suite.

My application is USB_Device/MSC_Standalone.

(I used HS-IN-FS workspace file so USE_USB_HS and USE_USB_HS_IN_FS are defined properly)

I run without any change,I can built program without an error.I downloaded and executed.

and program reached while(1).I connected USB cable to (CN14) but windows explore was not able to find mass strage device.

USB related registers were set below.

GOTGCTL= 3010000

GOTGINT=100000

GAHBCFG=  1

GUSBCFG=40001440

GRSTCTL=80000000

GINTSTS= 4008020

GINTMSK=c03c3814

GRXSTSR=      0

GRXSTSP=      0

GRXFSIZ=    200

DIEPTXF0_HNPTXFSIZ= 800200

HNPTXSTS=  80080

GCCFG=210000

CID=2100

GHWCFG3= 3eed2e8

GLPMCFG=      0

GDFIFOCFG= 3ee0400

HPTXFSIZ=      0

---- 0x4004 0800 ----------------------------

DCFG = 8200003

DCTL = 0

DSTS = 6

DIEPMSK = 0

DOEPMSK = 0

DAINT = 0

DAINTMSK = 0

DVBUSDIS = 17d7

DVBUSPULSE = 5b8

DTHRCTL = c100020

DIEPEMPMSK = 0

DEACHINT = 0

DEACHINTMSK = 0

HS_DIEPEACHMSK1 = 0

HS_DOEPEACHMSK1 = 0

---- 0x4004 0800 ----------------------------

DIEPCTL0 = 8000

DIEPTSIZ0 = 0

DOEPCTL0 = 8000

DOEPTSIZ0 = 0

Looks like DCFG register is incorrect.DSPD[1:0] = 11 means Full speed to work with internal FS PHY.

So I modified usbd_conf.c and stm32xx_ll_usb.c to select Full speed using HS.

After modification,I tetsted.Program.But It still has problem.

register were set below.

GOTGCTL= 3010000

GOTGINT=100000

GAHBCFG=      1

GUSBCFG=40001440

GRSTCTL=80000000

GINTSTS= 4008020

GINTMSK=c03c3814

GRXSTSR=      0

GRXSTSP=      0

GRXFSIZ=    200

DIEPTXF0_HNPTXFSIZ= 800200

HNPTXSTS=  80080

GCCFG=210000

CID=2100

GHWCFG3= 3eed2e8

GLPMCFG=      0

GDFIFOCFG= 3ee0400

HPTXFSIZ=      0

---- 0x4004 0800 ----------------------------

DCFG = 8200001

DCTL = 0

DSTS = 7ff02

DIEPMSK = 0

DOEPMSK = 0

DAINT = 0

DAINTMSK =

0 DVBUSDIS = 17d7

DVBUSPULSE = 5b8

DTHRCTL = c100020

DIEPEMPMSK = 0

DEACHINT = 0

DEACHINTMSK = 0

HS_DIEPEACHMSK1 = 0

HS_DOEPEACHMSK1 = 0

---- 0x4004 0800 ----------------------------

DIEPCTL0 = 8000

DIEPTSIZ0 = 0

DOEPCTL0 = 8000

DOEPTSIZ0 = 0

PCGCCTL = 0

ENUMSPD bit in DSTS register was 01,means reserved.So I was not able to connect to Windows explore.

Could you teach me how to set up these registers ?

If you have workaround software,please provide me.

If you need more info,let me know.

Best Regards,

Thank you.

Takao Kawai

tkawai1@gw.nsw.co.jp​

    This topic has been closed for replies.