Question
Use case: a pressure sensor which acts as an altimeter. At a place where there is a wide season change,does the LPS27HHTW provide the accuracy as mentioned in the Data sheet?My use case has critical implications and need an accuracy of about +1m (.12
Does it also give the mentioned accuracy during weather changes? (Use case is set up in Europe.)