Using FP-IND-PREDMINT1 for determining the frequency of vibration
Hello,
I am using FP-IND-PREDMNT1 and new to this . From the data website it says it is used for time and frequency domain signal processing and analysis of 3D digital accelerometers with flat bandwidth up to 6 kHz.
I wanted to know if is it possible to determine the frequency of a vibrating signal(constant but varying after some time 5-10 mins ) .
The frequency range is from 100-300 Hz.
Is it possible to get the exact frequency range from the FP-IND-PREDMNT1. Which software example?
Regards,
P