Question
using INT1 and INT2 of ism330bx for connecting with STEVAL-MKI245KA
Dear Sirs,
I would ask how it is connected ISM330BX with STEVAL-MKI245KA in the webinar. In fact STEVAL-MKI245KA has inside different sensors and I don't see the connector to plug STEVAL-MKI245KA.
Moreover in en.FP-AI-MONITOR2_V1.0.0_RC8 need to be installed in CubeMX?
The en.FP-AI-MONITOR2_V1.0.0_RC8 use one of INT1 and INT2 or both of ISM330BX?
Thanks