Skip to main content
Explorer
January 27, 2024
Question

Using STEVAL-MKI236A with UNICO GUI

  • January 27, 2024
  • 2 replies
  • 1329 views

Hello,

I have STEVAL-MKI236A (ASM330LHB - IMU) evaluation board, How can I make use of the UNICO-GUI to interface with the board. I do see the board listed on the GUI but how will I be able to interface with gui with just I2C without using the MOTHERBOARDs.

Thanks!

    This topic has been closed for replies.

    2 replies

    Technical Moderator
    January 29, 2024

    Hi @govindrzook ,

    Are you using the STEVAL MKI109V3?

    Explorer
    January 30, 2024

    Hello @Federica Bossi 
    I am not making use of STEVAL-MKI109V3 motherboard and currently directly using the evaluation board via SCL, SDA pins of I2C interface. is it possible to make use of the UNICO-gui without that motherboard?

    Please advise thanks!

    Technical Moderator
    February 1, 2024

    Hi @govindrzook ,

    Yes, as explained in our official page, it is available for three operating systems: STSW-MKI109L for Linux Debian-based; STSW-MKI109M for Mac OS X; STSW-MKI109W for Windows.