Using the STM drivers with kernel above 6.6 i.e 6.13
Hi,
im currently working on interfacing the STM mems sensors with Beagle Vahead board, im using a kernel version of 6.13 and i tried patching the STM MEMS IIO drivers from link. Im aware that the STM has confirmed the testing of the driver with kernel 6.6.
While patching i faced few errors ie mis match in the headders and i have successfully resolved them.
im able to boot the device and able to get the device node in the /sys/bus/iio/device when interfacing the lps22df sensor.
when any other sensors (lsm6dsox, lisduxs12,lsm6dsv32) are interfaced on the same bus, im not able to detect the device. i have the same hardware set for lps22df also. but in that case i was able to get the raw pressure and temperature data.
I want to understand the issue why it happens so.
i have mentioned the mininal properties on the i2c bus node in DTS file. and have omitted all the optional parameters.
have a look at the STM driver booting errors
[ 1.143802] st_lsm6dsox_i2c 2-006b: supply vdd not found, using dummy regulator
[ 1.168768] st_lsm6dsox_i2c 2-006b: supply vddio not found, using dummy regulator
[ 1.177306] st_lsm6dsox_i2c 2-006b: probe with driver st_lsm6dsox_i2c failed with error -121
[ 1.186313] st_lsm6dsvx_i2c 2-006a: supply vdd not found, using dummy regulator
[ 1.194100] st_lsm6dsvx_i2c 2-006a: supply vddio not found, using dummy regulator
[ 1.202116] st_lsm6dsvx_set_page_access set page access error
[ 1.208680] st_lsm6dsvx_i2c 2-006a: probe with driver st_lsm6dsvx_i2c failed with error -121
[ 1.217828] st_lps22df_i2c 2-005c: failed to read Who-Am-I register
[ 1.224226] st_lps22df_i2c 2-005c: probe with driver st_lps22df_i2c failed with error -121
[ 1.235138] Legacy PMU implementation is available
copy of dts file where it is defined