Using X-CUBE-MEMSMIC1 without X-NUCLEO-CCA02M1
Hello, I am trying to record audio with external digital PDM microphones using the MEMSMIC1 example but it is not so straightforward without the nucleo expansion board. Because the CCA02M1 has a direct connection to the pc it is able to be detected as a microphone in the device manager, it is easily used through audacity. How can I implement this project and use audacity with my microphone setup if they are directly connected only to the development board (I am using nucleo-wb55rg)?