Valid range (Full Scale) for the gyroscope (LSM6DSOX) in a health tracking device
Hello,
my team is planning to use the gyroscope of the part LSM6DSOX in a health tracking device,
and one of the engineers noticed that the readings from the Gyroscope often have measurements that go beyond ±2000dps (specified in the datasheet as Full Scale).
When converting raw data to dps, based on the Angular rate sensitivity, 2000dps would correspond to around 2000dps/70mdps ≈ 28,571 (raw data). But there are raw data readings higher than 28,571.
The datasheet does not cover results beyond ±2000dps.
Is there any validity for readings beyond ±2000dps, to the point of
for example using the given Angular rate sensitivity to convert raw data output of 32767 to ≈ 2,293dps (15% beyond Full Scale)?
Or could there be any distortion involved, making readings beyond 2000dps invalid?
Best Regards,