values of iis3dwb mems
I am reading the x, y, z axis values of iis3dwb mems using DSP Microprocessor.
However, the following results are displayed.
lpf or 2g, 4g, 8g, 16g change the same
I want to ask if the procedure is wrong
X auxi : red graph
initial(default) value : 39xx.xxxxxx ~ 3996.xxxxxx(mg)
Q1) How to set the initial value to 0?
Value changes rapidly even without vibration.(0g ~ 3g)
Even if there is vibration, the value changes rapidly.(0g ~ 3g)
Q2) How to make the rate of change small?
It is not a program error.
Q3) Is the sensitivity of the original iis3dwb like this?