Question
VL53L0X interrupt setting
Posted on May 21, 2018 at 06:53
Hi
I am trying to get the VL53L0X using the api provided and the source code available on
https://os.mbed.com/users/andcor02/code/vl53l0x_api/
which is just a copy of the VL53L0X api. I am using the STM32L432KC NUCLEO board with I2C connnection to a breakout board available on ebay ->The module works fine but the interrupt pin does not do anything. I am trying to use the 0x04 setting for NEW_DATA_READY setting as per the API, but don't see any trigger on the interrupt or on a digital logic analyzer.
Please help
Best
Chandra