Vl53L0X Offset Calibration
Hello,
I am currently trying to implement offset calibration to VL53L0X sensor. I placed sensor in front of white paper with 100mm distance as datasheet suggest. When I get sensor measurement before offset calibration, I get 135mm which is fine because i placed glass in front of the sensor. However, when I calibrate sensor, I get 0mm as a result from same distance. So, I move sensor to 200mm, I am getting 100mm for measurement. I think of offset calibration as it will add or subtract offset value from the measurement value not set 0mm when the offset calibration has made. I am using VL53L0X_perform_offset_calibration function from api. I followed UM2039 documentation as referance. So, what could be the possibble reason for that or is it the way offset calibration work?
Regards,
Taha