Skip to main content
Visitor II
September 19, 2019
Question

VL53L0X running on a 3.3 voltage rail

  • September 19, 2019
  • 3 replies
  • 1147 views

We have designed a circuit using this chip with the 3.3 voltage rail . Without converting it to 2.8 as it is bellow the max thresh-hold as per the datasheet.

We also pulled up the XSHUT pin high to 3.3v using a 10k ohm resistor. In theory it should put the device into a software standby state. But the device doesn't turn on.

The only way we were able to turn on the device on was directly connecting the 3.3 v to the XSHUT pin, but it fails to do any sort of ranging.

We followed the Application schematic, described on the datasheet.

Any help will be greatly appreciated.

    This topic has been closed for replies.

    3 replies

    Visitor II
    November 26, 2019

    any news on that issue?

    TashfiqueAuthor
    Visitor II
    January 9, 2020

    switched over to vl6180x and put a Voltage Regulator ...

    Visitor II
    February 7, 2020

    We are using VL53L0X with 3.3 V rail and 10K pull-up resistors and it works. Perhaps its life span will be shortened.