Skip to main content
Visitor II
April 11, 2018
Question

VL53L0X Time-of-Flight Distance Sensor ''FOV''?

  • April 11, 2018
  • 1 reply
  • 3118 views
Posted on April 11, 2018 at 09:45

The specifications of the sensor states a 'FOV of 25 degrees'. I'm not really sure what that FOV means here. The beam is reflected back to the detector and filtered by a pinhole. There's a pinhole, so what would be the point of such a high divergence, if that is what FOV means?

If 'FOV' is the divergence and if the divergence is artificially increased so it will reach the pinhole which is at an offset to the emitter it seems too much much even for few cm distances, right?

I also do not see how the high divergence will help detect objects at other angles (provided this is the purpose) besides the one the pinhole is pointing at as any reflected ir light with a slightly different angle will be physically cut and not reach the sensor inside the pinhole. Even if there wasn't a pinhole any non retroeflective surface not in the center of that FOV still wouldnt work unless it was in the middle of the 'FOV', in my understanding.

My only explanation why there is a large divergence is simply adding a collimating lens in front of the laser was not needed as the laser was bright enough to work without it and would just add to the cost. But then the question arises why not have a pinhole in front of the laser emitter in the first place and why have a 'FOV of 25' specified in the specifications if it doesn't mean anything. Plus this still may give wrong readings for retroreflective surfaces as many beams from very different distances and any angle in the '25 degree FOV' may manage to travel back to the pinhole.

So I don't understand this '25 degree FOV' and its purpose.

    This topic has been closed for replies.

    1 reply

    ST Employee
    May 7, 2018
    Posted on May 08, 2018 at 01:34

    the 25 degree Field of View, can be thought of as a cone of light. The diameter of the illuminated 'spot' is approx. 1/2 the distance away from the sensor. The VL53L0X has no optics. The 25 degrees is the result of the properties of the Vertical Cavity Surface Emitting Laser (VCSEL) used by the chip. Putting a lens on the transmit side of the chip is not recommended as it would affect the eye-safety of the device. Please don't do it without going through the full FDA eye-safety testing.

    Putting a lens on the receive side IS a good idea. ST did it and created the VL53L1X, which started shipping late Q1 2018. By putting a lens on the device the sensor can detect where the photons came from and allow you do more.

    The VL53L1X can reduce the field of view to 10 degrees for instance, or look only on one side or the other.

    The addition of the lens does cost more, but not much more. Makes the chip a bit taller though. The two sensors have the same footprint.