Question
VL53L1X: Is there only one kind of calibration (API), or there is a calibration that is made by ST for their dev. and breakout boards?
When I use the breakout board included in the dev kit, the precision is at most 2 mm, but when I use the VL53L1X soldered on one of my board, the precision is really different. Is there a particular calibration or setting that are input to the breakout board that would make it this way?