VL53L1X Low Temperature Performance
We using the VL53L1X in an application where it will be mounted in a manner that's protected from sunlight, but exposed to cold ambient temperatures - -40°C and possibly lower. The VL53L1X datasheet has a lower operational temperature limit of -20°C and I'm wondering how the sensor behaves below this temperature? Is it possible to use this sensor below -20°C?
Will the data coming off of the sensor have distinguishable characteristics if we're below the minimum operational temperature?
When I read through the form, there are many posts talking about this sensor being meant for indoor applications and to avoid sunlight as that causes issues with the sensor. I'm assuming this is why the sensor is only rated to -20°C.