VL6180X wrap-around filtering: is this possible without the API?
Hello,
I'm working on a project with a VL6180X ranging sensor, and I'm running into the problem that it responds to reflective surfaces far beyond the desired range (100 mm) - e.g. it picks up reflective stripes on the jackets of emergency personnel at over 1200 mm (4 feet) distance, rendering the whole thing unusable.
The datasheet mentions a Wrap-Around Filter (WAF) to solve this problem; however, it turns out that this filter (and only this filter) requires the use of the VL6180X API - which is a problem, as I'm using a simple PIC controller for the overall functionality (switching on a small liquid pump when a hand is within range).
I already checked out the API, but it isn't clear at all how this WAF works. Could someone shed some light on this? If it is merely a matter of setting a bunch of registers, my controller should be able to handle that just fine; and even if some continuous external processing is required, it shouldn't be impossible.
(I also looked if I could simply decrease the VCSEL output to limit the range, but there seems to be no register setting for this.)
What I don't want, is to redesign and rebuild the hardware and software in order to be able to use just this one feature.
Thanks already for any help!
Richard