Skip to main content
Visitor II
July 30, 2024
Question

Wake-Up current of IIS3DWB

  • July 30, 2024
  • 0 replies
  • 524 views

I am making my own wake up interrupt program based on P16 of the application note, and it is working fine. However, I noticed that I have to enable IIS3DWB to use the wake up function, which increases the overall standby current of the system by about 1.1mA. That is not what I was expecting, as I thought that the wake-up function would run at a very low current.
So is there a way to reduce the current consumption of the IIS3DWB when using its wake-up function?

    This topic has been closed for replies.