What are the typical ODR deviations (Clock deviations) in the ISM330DHCX and other iNEMO Modules and is it somehow possible to connect external clocks?
Hello,
In our application we've found quite big differences in ODR between different samples of the ISM330DHCX and also for different modes:
For example if setting the ODR to 416 Hz we measure > 440 Hz. Furthermore when only ACC is active the ODR is 440 Hz, when GYR and ACC are active the ODR drops to 425 Hz. Is there any way to connect an external clock source or to somehow synchronize the ODR to an external clock? What are the specifications for ODR deviations for ISM330DHCX and LSM6DSOX for example? Is there any way to make ODR more stable?
Thank you!