What could cause the LPS22HH boot phase to never finish?
I am evaluating the LPS22HH for a product, but the device acts a bit unreliably. After power-on, sometimes the BOOT_ON bit in INT_SOURCE (24h) is never cleared.
I wait for at least 500ms before checking the BOOT_ON bit, so that should be plenty of time for the pressure sensor to finish the boot phase. Repeated readings at the same interval show the bit is still set and never seems to be cleared.
What could cause the device to get stuck in the boot phase?