What frequency Should I use for 48khz audio sampling with SAI Interface
I am using a stm32wb55 and I want to acquire PDM data from a MEMS microphone and convert it into PCM. I want to use the SAI PDM interface.
I have a doubt about the frequency I should put there :
I want to use a decimation of 64. In the reference manual I see this (under the chart it's written that the values are found using decimation of 64) :
As I want to record one microphone with 48kHz and 64 decimation, 3.072 MHz makes sense (48k*64) but I am confused by the 6.144 MHz in the reference manual.
In the first picture, should I put 3.072 or 6.144 ? I think that my microphone only accept between 1MHz and 3.5 MHz. Also, if I try to put 3.072 MHz, the only solution found by cubeIDE is 3.20 MHz. Any solution to this or do I have to work with 3.20MHz (in the case 3.072MHz is the way to go) ?