Skip to main content
Visitor II
July 9, 2019
Solved

What in-circuit debugger/programmer should I use for STEVAL-MKSBOX1V1?

  • July 9, 2019
  • 7 replies
  • 5428 views

I am using STEVAL-MKSBOX1V1 and I want to do some changes in the firmware.

What in-circuit debugger/programmer should I use? Should I use ST-LINK/V2 or STLINK-V3SET or STLINK-V3MINI?

Please help me. Thank you

    This topic has been closed for replies.
    Best answer by Eleon BORLINI

    Hi @Eugene Agustin​ , if programming through JTAG/serial wire debugging (SWD), I suggest you to use the ST-LINK/V2 programmer because of 1.8V level compatibility with ,ow power STM32L4R9. The HW connection is the connector numbered "8". Board schematic will be available soon on st.com. Regards

    7 replies

    Graduate II
    July 9, 2019

    Manual says "The board includes the ST-LINK V3 (with UART pins for debugging) compatibility."

    Unfortunately no pictures of the back side of the board.

    Suggest you contact your local sales office and discuss.

    Visitor II
    July 9, 2019

    Here is the back side of the board.

    Please look at the attached image thank you

    Technical Moderator
    July 11, 2019

    No picture attached. Make sure you upload and insert it.

    Visitor II
    July 12, 2019

    Sorry I forgot to insert.

    Thank you

    Visitor II
    July 12, 2019

    0690X000009YY8cQAG.png

    ST Employee
    July 15, 2019

    Hi @Eugene Agustin​ , if programming through JTAG/serial wire debugging (SWD), I suggest you to use the ST-LINK/V2 programmer because of 1.8V level compatibility with ,ow power STM32L4R9. The HW connection is the connector numbered "8". Board schematic will be available soon on st.com. Regards

    Visitor II
    July 16, 2019

    Hi @Eleon BORLINI​ ,

    I already bought an ST-LINK/V3 since it is the newer version. Am I right that it will work on SensorTile.box for programming?

    Thank you

    ST Employee
    July 24, 2019

    Hi @Eugene Agustin​ , please consider this note, as reported in the SensorTile.box user manual:

    >> Note: Your ST-LINK must have the level shifter to function at 1.8 V (the SensorTile.box power supply).

    This mean that you should use by now either the STLINK V2 which is 1.8V compatible or the STLINK V3 with level shifters from 3.3V to 1.8V. If you already have a Nucleo board, you can use the onboard JTAG programmer (which is a STLINK V2). However, please consider that an adapter board from STLINK V3 to SensorTile.box will be soon available online.

    Another way to program the SensorTile.box is through the dfu mode: you can build your FW and generate the .dfu file, which can be downloaded on the SensorTile.box through the DfuSe. Not the best way to do a debug but it should be only a temporary patch.

    Regards

    Visitor II
    July 22, 2019

    Hi @Eugene Agustin​ did you find an answer to your question?

    I know the STLINK-V3SET is compatible with the MKSBOX1V1 as per this post.

    This document compares STLINK-V3SET and STLINK-V3MINI on Page 2.

    Visitor II
    July 23, 2019

    Hi @DIM​ 

    Not yet.

    Thank you for sharing the information. I need some quick start guide or manual on how to use STLINK-V3SET on MKSBOX1V1.

    ST Employee
    August 2, 2019

    Please note for the sake of completeness that you can now find the Sensortile.box schematic online. Regards

    Visitor II
    April 13, 2020

    Anything new about adapter board with dedicated level shifters and LDOs for the 1.8V debugging?

    In UM2448 chapter 12 B-STLINK-VOLT board extension description shows this but actual board is still missing.

    ST Employee
    April 14, 2020

    Hi @savimakt​ , good question... I added the ST-LINK Utility and the STLINK-V3 topics to the original question for eventual support. Regards