Skip to main content
Visitor II
February 4, 2014
Question

What is the clock frequency where the mics switch from normal mode to sleep mode?

  • February 4, 2014
  • 2 replies
  • 542 views
Posted on February 04, 2014 at 16:57

What is the clock frequency where the mics switch from normal mode to sleep mode?

    This topic has been closed for replies.

    2 replies

    Visitor II
    February 7, 2014
    Posted on February 07, 2014 at 11:27

    Actually the threshold of the switch between normal mode and sleep mode is not fixed. There is an hysteresis. In fact the microphone changes its behavior when the clock frequency is comprised between 500kHz and 700kHz

    Regards,

    Alessandro

    Visitor II
    February 7, 2014
    Posted on February 07, 2014 at 11:30

    Addition to previous statement.

    Basically the microphones switches off when the clock frquency decreases to value lower than 500kHz but switches on for frequencies over 700kHz.

    Alessandro