Skip to main content
Visitor II
March 21, 2018
Question

What is the difference between normal mode and low-power mode for lis3de

  • March 21, 2018
  • 1 reply
  • 782 views
Posted on March 21, 2018 at 07:58

I know for lis3dh, the normal mode gives 10-bit resolution while the low-power mode gives 8-bit resolution. But for lis3de, both normal mode and low-power mode gives 8-bit resolution. So what's the difference between them.

Also the following picture shows ODR 1.6KHZ is not supported by normal mode and low-power mode can achieve larger maximum ODR as 5.376KHz while in normal mode it's only 1.344KHz. T

hat means if I want to achieve ODR up to 5.376 kHz, I have to use low-power mode? This gives me higher ODR and lower power? But what do I lose?

0690X0000060ABhQAM.png
    This topic has been closed for replies.

    1 reply

    March 21, 2018
    Posted on March 21, 2018 at 08:26

    Hello,

    Have a look at this official answer:

    https://community.st.com/0D50X00009XkfQYSAZ

    David

    Kefei YaoAuthor
    Visitor II
    March 21, 2018
    Posted on March 21, 2018 at 10:46

    OK. Although it looks a little bit weird but anyway it address my question. Thanks for the direction.