What is the MotionFD input data frequency tolerance? (is it possible to use data from LSM6DSO FIFO)
Hi,
We are currently evaluating the possibility of using the LSM6DSO and LPS22HH with the MotionFD library, to detect when our product has been dropped from height (up to 9 meters).
One of our requirements is that the product always monitors for fall events even when the main MCU is off/standby. Seeing as we do not need a real time indication of a fall event (just keeping a log of events), we want to try and utilise the FIFO buffer on the accelerometer to collect data that can retrospectively be passed to the MotionFD algorithm for analysis.
According the the MotionFD user guide (https://www.st.com/resource/en/user_manual/dm00427990-getting-started-with-motionfd-realtime-fall-detection-library-in-xcubemems1-expansion-for-stm32cube-stmicroelectronics.pdf), the library requires "accelerometer and pressure sensor data sampling frequency is 25 Hz".
Upon review of the LSM6DSO datasheet, it was found that the closest batching data rate that can be used for the FIFO is 26 Hz. Will this mismatch be a problem for the fall detection algorithm?
Many thanks
Calum