What is the peak-to-peak 'g' expected on a IIS3DWB accelerometer when device is completely stationary?
Hello
Sampling data from the IIS3DWB accelerometer over the course of a couple of seconds, when the device is completely stationary, on the 16g range, the peak-to-peak readings on each axis are:
p2p x = 0.0566g
p2p y = 0.0634g
p2p z = 0.1215g
These seem to be quite excessive detected movements; and assumed it was the noise floor (!!!) of the device. A bit of digging on these forums suggested enabling the LPF2; which I did, at ODR/100. The results improved, to:
p2p x = 0.0151g
p2p y = 0.0122g
p2p z = 0.0166g
But these too still appear quite large given the completely static nature of the device.
Are these results to be expected? Is this the noise floor of the MEMS device, ADC, other internal circuitry?
Kind regards
Gary Partis