when i connect the x-nucleo-iks01a2 board to the p-nucleo-lrwan1 dev kit i get PHY txtimeout error even do the frist payload does reach the application but no others do.
Hi,
I am following manuals UM2084 and UM2073 and with out the iks01a2 board everything thing works fine with the ***** payload reaching the application over the web every-time, but when i reset up and add the iks01a2 board to the dev kit i get PHY txTimeOut in the terminal window for every tried tx no rx happens when i get this error, also the very frist payload reaches the application but no others do when this error happens. In the i-cube-lrwan software i am using the end node demo and in the hw_conf.h file i do un-comment the sensor_enable define which following the manual should get it to work and i am using keil as the toolchain for compiling and flashing the dev kit. Please help or if anyone knows a better more definitive guide to follow please share as searches seems to bring up no answers. thx in advance.