Skip to main content
Visitor II
December 9, 2021
Question

When I plug my STEVAL-MKI109V3 card into my computer, the port is not defined. I am using windows 10.

  • December 9, 2021
  • 4 replies
  • 1699 views

0693W00000Ho0BlQAJ.png

    This topic has been closed for replies.

    4 replies

    Technical Moderator
    December 9, 2021

    Welcome, @AGonc.3​, to the community!

    The kit communicates via a virtual COM port. For this you had to install a driver before W10, but since W10 this is no longer necessary because the driver is already included in W10.

    On your screenshot you can see the STM32 Virtual ComPort under Other devices with an exclamation mark in a yellow triangle, so this problem must first be eliminated. Did you accidentally install the VCP, which is only intended for W7, W8 etc?

    Regards

    /Peter

    AGonc.3Author
    Visitor II
    December 9, 2021

    I downloaded 2 different versions given on the site and ran both of them, and I encountered the problem with the image I added earlier in both. Do I need to install any driver? is there a reliable site you recommend for this?0693W00000Ho2kPQAR.png

    Technical Moderator
    December 9, 2021

    As already mentioned, no driver is required for W10.

    What is the error message at the STM32 Virtual ComPort under Other devices showing an exclamation mark in a yellow triangle?

    Regards

    /Peter

    AGonc.3Author
    Visitor II
    December 9, 2021

    0693W00000Ho2nmQAB.png

    Technical Moderator
    December 9, 2021

    What is your version of W10?

    You'll find it using the command winver.

    Regards

    /Peter

    ST Employee
    December 9, 2021

    Hi @AGonc.3​ ,

    did you installed the ProfiMEMSToolV3.22.2_00_08000000.bin firmware on the STEVAL-MKI109V3?

    You can find it in the \FIRMWARE\ProfiMEMSTool board folder.

    -Eleon